Specification-compliant configuration of the OPC UA Server Permalink

To operate the OPC UA Server according to the OPC UA specification, the following settings are required:

  1. The ⮫ City location has to be configured for the certificate.

  2. An OPC UA Server certificate has to be generated

  3. The CRL checks ⮫ EnableCRLChecks have to be enabled.

  4. The ⮫ CommunicationMode has to be set to ‎MIN_SIGNED‎ or ‎SIGNED_AND_ENCRYPTED‎.